MOVE.TARGETPOS

Description

MOVE.TARGETPOS specifies the target position for an absolute (MOVE.GOABS) move. MOVE.TARGETPOS is an absolute position referenced to the electrical home position (the position where PL.FB = 0).

Set MOVE.TARGETPOS before initiating a MOVE.GOABS.


  • MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.

General Information

Type

R/W

Units

Depends on UNIT.PROTARY or UNIT.PLINEARUNIT.ACCLINEAR

Rotary: counts, rad, deg, (Custom Units), 16-bit counts

Linear: counts, mm, µm, (Custom Units), 16-bit counts

Range

N/A

Default Value

N/A

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1146

Yes 64 bit Yes

M_01-05-11-000

Related Topics

MOVE.GOABS